Hi ti team,
在产品老化时,TPS61288会出现输入MOS击穿情况,请帮忙分析下,Thanks!
测试条件:Vin=3.3V-10V Vout=13V1A
原理图如下,请问 1UH电感是否合适?规格书有推荐1uH感值(如第二张图),3图是目前使用电感规格

2图

3图

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
感量略有偏差问题不大,重点在于电感饱和电流足够,按照你提供的规格8A是足够的。如果选择2.2uH, 纹波电流略微小一些,相对比1uH要略微安全,但并没有问题。
你需要确认输入电压是否稳定在3V以上,以及负载是否会超过1A, 如果出现最恶劣的情况如输入电压因为波动低于了3V, 而负载超过1A, 就有可能出现超高的输入电流,有可能导致电感饱和。 所以你需要确认输入电容足够大,并且layout上尽量靠近功率电感。