This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92662-Q1: CCPx电容的作用

Part Number: TPS92662-Q1


设计师

你好

1、请教一下,CCPx引脚的外部100nF电容的作用,是否是内部集成开关MOS的驱动电路的自举电容?

2、这个电容的充电回路;

3、以及这个电容的放电回路;

4、对于某个内部集成mos通道,是否可以处于常开或者常闭的状态,也就是占空比100%或者0%输出。

谢谢