您好~
我們客戶端在詢問,為什麼Remain Capacity更新為0後,SOC尚未變更為0,約等待10秒後SOC才更新為0。從系統提供的Log電壓、電流...等等數值都一直有update,不像是通訊失效。
下圖是我們系統讀取的Log資料,每秒紀錄一筆Log:
我們已知Remaining Capacity更新為0的原因(Term Min Cell V),但不知道為什麼SOC沒有同步更新為0,請協助告知!!!
謝謝~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好~
我們客戶端在詢問,為什麼Remain Capacity更新為0後,SOC尚未變更為0,約等待10秒後SOC才更新為0。從系統提供的Log電壓、電流...等等數值都一直有update,不像是通訊失效。
下圖是我們系統讀取的Log資料,每秒紀錄一筆Log:
我們已知Remaining Capacity更新為0的原因(Term Min Cell V),但不知道為什麼SOC沒有同步更新為0,請協助告知!!!
謝謝~
Hello,
What does 5690 mean?
A: 5690 = 56.90 Celsius
The RSOC_HOLD is not set.
Attached is our final product's gg file and drone BMS log.
您好,可以尝试下面的方法改进RSOC jump问题:
1- change load select to 1, this uses the present average discharge current.
2- Enable smoothing
3- DO not set RSOC_HOLD and Smoothing at the same time
4- Set Term Voltage to the steep zone of the OCV profile.
您好,The SOC reporting 11 when the cell-1 is 2.6V could be related to the delay of 10seconds.
Another reason could be that the end of discharge voltage falls under the flat region. I will need to know the matched ChemID. You can provide the srec, or they can read ChemID (see below)
As for the voltage imbalance seen above, is cell balancing enabled? Doing a sanity check in the schematic will also help identify this