This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25172: BQ25172使用

Part Number: BQ25172


采用BQ25172,麻烦帮忙看下如下问题

1、三节镍氢的话,VIN电压是多少?是大于1.7V*3+Vsleep约为5.235V么?
2、正常情况下过电压阈值是1.7V*3么?如果VIN是5V的话,那这样阈值电压是不是相当于5V-Vsleep,大概是4.865V?5V的VIN会有什么影响呢?

  • 您好,The input voltage needs to be higher than the battery voltage + sleep threshold and less than the input over voltage threshold for the device to charge. In your case with 3S NiMH battery, the typical VIN min value will be 1.7V*3 + 0.135V to fully charge the battery.