After the protected MOS tube is over-temperature protected, the charging and discharging MOS tube is turned off, and a multimeter is connected in it. There is a current of about 12MA, and then it slowly decreases. The direction of the current is as shown by the arrow in the figure. Why is there still this current after the charging and discharging MOS is turned off?
保护的MOS管过温保护后,充放电的MOS管关闭,串一个万用表进去,有12MA左右的电流,然后慢慢降低。电流方向如图箭头所示,请问充放电的MOS关闭后为啥还有这个电流?