This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: BQ76952 大电流放电时断开放电MOS AlarmStatus 状态中FULLSCAN不再置1除非重新复位BQ76952

Part Number: BQ76952


BQ76952  在电池系统中,电池是16串的,电压是52V左右,现对此电池进行放电 使用的是30A电流,电池连接逆变器且逆变器带1500W的负载;放电的时候断开放电MOS,此时单片机时时读取BQ76952 AlarmStatus 0x62状态寄存器,返回的结果中FULLSCAN不再置1;没有在前面的那些操作时定时读取AlarmStatus 状态都是有FULLSCAN置1;FULLSCAN状态对我们程序来说很重要,程序中是根据此状态来显示电池单体电压电流等信息;

在出现此问题时,我们把BQ76952其他很多寄存器值都打印出来看,打印出来的寄存器值都是正常的;此情况对我们产品的影响是致命的,希望可以得到你们的帮助