This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3525A: 我打算采用此芯片做一款推挽升压电源,变压器原边采取12V7AH铅酸电池供电,副边分时输出DC110V,DC75V,疑问如下

Part Number: UC3525A

1.反馈环路不变,单片机分时控制芯片的2脚的参考电压

  上电3秒内时,单片机GPIO1输出0,则芯片2脚电压为5.1V左右,此时Vo输出110V

 上电3秒后,   单片机GPIO1输出1,则芯片2脚电压为3.4V左右,此时Vo输出75V

请问这种接法的时候,2脚参考电压是否高了,或者运行的过程中不要改变2脚电压?

参考别家产品2的电压是2,5V~2,6V且整个过程中电压不做改变,只改变Vo输出反馈回来的参数

2.芯片的1脚到芯片的9脚之间电阻取值的规则是什么?是否需要并RC电路或者串RC电路?

 

误差放大器的9脚电压是否可以在2.5到5.1电压范围之内?

其他问题如下:

1.升压输出是否需要反并续流二极管?

2.PCB layout需要注意什么?

3.误差放大器的接法是按普通的运算放大器接还是按比较器接?

4.怎么防止误差放大器自激振荡?

5.有没有关于UC3525的官方例子供参考?

推挽升压电路基本如下

谢谢!