设计TPS7A4700电路如上
实际测量时,发现其输出电压是5.075V,而不是5V,请问是为什么呢
按照设计,输出电压应该为1.4V(REF)+ 0.2V + 3.2V = 5V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

设计TPS7A4700电路如上
实际测量时,发现其输出电压是5.075V,而不是5V,请问是为什么呢
按照设计,输出电压应该为1.4V(REF)+ 0.2V + 3.2V = 5V
HI
LDO输出精度在2.5%范围内都是正常的,所以输出是一个范围值4.875~5.125V, 都是正常的。
有一点需要注意下,上面用于电压设置的GND建议是noise较低模拟GND,与输入输出用的GND隔离开(在芯片底短接,可以参考datasheet).