Part Number: LM5176
我想使用LM5176设计一款输出为5V-28V 5A的电源。请问Comp补偿环路应该如何配置比较合适?
我尝试了使用web设计器给出的5V补偿环路,但是升压到20V时会出现纹波过大以及跟随速度不够导致输出被拉死的问题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
按照你这种情况一般补偿设置在输出范围中间值,即16.5V, 只是有外部补偿的控制芯片不适合做大范围的输出可调,否则就会出现你提到的情况,因为输出电压和补偿对应的电压距离较大,造成环路不稳定,就会纹波异常(也就是如上补偿对应5V,环路稳定,但是补偿就不适合28V)。
如果板子已经做出来了,如上补偿设置在对应电压16.5V. 如果此时纹波还是超过你的预期,只能在输出增加一级LC(磁珠加电容)。
或者建议你选择没有外部补偿的电源芯片,只是大功率的升降压芯片,并且没有外部补偿电路的芯片极少。