Other Parts Discussed in Thread: BQSTUDIO, EV2400
为什么BQ76952配置寄存器 或者用BQStudio上位机来写入配置 修改SETING里面的寄存器值 改了后 WIRTE TO DATA MEMORY 还是没有用 还是之前的值 在读取 readall 还是全部是默认值 为什么写入总是失败
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请确认是否进入保护,或者seal mode
您好,写参数时将autoscan 关掉,再试一下,将完整的register画面发过来看一下。
您好,请将整个BQSTUDIO的画面发过来看一下。左下角的红色提醒内容是什么
您好,建议您用EV2400通讯试一下。不建议将 EV2300 与 BQ76952 一起使用。为了确保与 BQ76952 系列的兼容性,对 EV2400 固件进行了多次更新,因此使用 EV2300 时可能会出现一些不明显的问题。
您好,正在查看,稍后回复。
您好,请参考下面内容
I recommend reading the BQ769x2 Software Development Guide for some examples of communicating with the device.
Could you provide more details about these captures? Specifically what commands the host is trying to send in each capture. Also, it looks like the last capture is zoomed out too much so that the bytes are not fully displayed.
One thing to note is that bqStudio will normally handle entering and exiting config update mode and sending the checksum when writing to registers. It may appear different due to this.