做一个低功耗的设备,最大电流20mA,选择TPS62736,样板刚开始没事,后来发现功耗大,发现TPS62736不起作用,只比输入电压小一点,单独测试发现挂了。供电电压是锂电池,最大是4.2V,是不是冬天静电多,击穿了mos
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
做一个低功耗的设备,最大电流20mA,选择TPS62736,样板刚开始没事,后来发现功耗大,发现TPS62736不起作用,只比输入电压小一点,单独测试发现挂了。供电电压是锂电池,最大是4.2V,是不是冬天静电多,击穿了mos
Hi
注意芯片底部的PowerPad需要与GND充分焊接(不连接GND,很容易造成芯片损坏)
另外PowerPad要做散热设计,用PCB上大面积的GND铜铂用做散热片。
Hi
另外不要做带电操作,例如直接在没有保护时,直接插拔电源等等。
这个还真是带电插拔了。刚开始样机功能跑通,发现软件有BUG,功耗还是偏大,不知道怎么就挂了。平时调试有一个电源板,上边有常用的电压,一般是通过开关上电,很多时候也会热插拔,按理说有充电芯片在前边扛着,对62736影响不大吧
关键是不知道怎么坏了,随机比较强,偶尔两个坏了也不知道怎么回事。其他的都没事,坏的3个测试电压只比锂电池电压低0.1--0.2V,这个只能是MOS管直接导通,芯片里边电压转换已经不起作用了。
刚开始焊接了12块样机,测试都没有问题,输出都符合要求,因为是低功耗蓝牙设备,功耗不达标,就继续调程序。其他的设备都在桌子上放着,由于设备尺寸只有22mm,不可避免用手摸。现在终于把设备功耗调好,蓝牙广播模式外带测温及往flash里写数据,平均功耗在十几二十多uA。整个板子感觉不到发热,即使短路,也只会损害锂电池充电芯片。批量做带外壳保护会好些,我的测试发现即使TPS62736坏了,因为后路还是有输出,整个系统一样工作,但有一个小忧患没解决,理论上TPS是不会坏的,总想找到坏的原因。