This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2776: LM2776无法供电

Part Number: LM2776


目前,我所使用的方案如下:

使用LM2776输出-5V,经过π型滤波后,给40颗运放提供负电源,在上电后,LM2776不输出-5V,于是,我做了以下实验:

1.去掉π型滤波,将-5V直接给运放供电,LM2776不输出-5V;

2.示波器没有测到上电瞬间的-5V的毛刺或者变化,也没有测到-5V电流的突变波形;

3.去掉LM2776模块电路,使用外部可编程电源提供-5V,没有问题,电流显示44mA;

4.去掉一半数量左右运放,LM2776正常输出-5V;

5.在π型滤波后增加一颗10欧姆电阻,LM2776正常输出-5V;

请问下,以上实验似乎说明LM2776电流可能在上电时不够,但是我也没有测到相应波形,想问下可能是什么原因造成以上现象呢

  • Hi

         5.在π型滤波后增加一颗10欧姆电阻,LM2776正常输出-5V;  如果此时没有带运放负载的话,说明芯片带载50mA可以正常工作,超过所需要的44mA,  但实际上带载运放后无法正常工作,说明瞬态电流需求有可能超过200mA.

         尝试将LM2776输出电容增加到10uF甚至22uF看带载能力是否有改善。