Other Parts Discussed in Thread: TMS320F2800137, UCC27284
我们最近在使用TMS320F2800137(MCU)+UCC27284(栅极驱动器)+CSD19506KTT(MOS)驱动电机,但是电机转不起来。在MOS的漏极开路时,MOS输入波形如下(黄色为高侧):

MOS漏极接上30V电压时,MOS输入波形如下:

但是电机转不起来。原理图如下:
删除图中的D2,C4,C6以及将R6改为0欧姆,现象依然存在。请帮助看看硬件问题,谢谢!


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们最近在使用TMS320F2800137(MCU)+UCC27284(栅极驱动器)+CSD19506KTT(MOS)驱动电机,但是电机转不起来。在MOS的漏极开路时,MOS输入波形如下(黄色为高侧):

MOS漏极接上30V电压时,MOS输入波形如下:

但是电机转不起来。原理图如下:
删除图中的D2,C4,C6以及将R6改为0欧姆,现象依然存在。请帮助看看硬件问题,谢谢!


现在这个波形基本正常了。但是还是转不起来。但可以明显感觉到电机周期性的动一下(就像周期性打嗝一样),但是就是转不起来。另外我们发现输入驱动器的方波波形占空比20%,经过UCC27284后,波形变成了50%的方波,这是为啥?而且驱动器输出波形还有一个明显的台阶,不知为何?请指教。谢谢

经过进一步确认是高侧方波经过驱动器后变成了50%占空比的方波 而低侧方波还是输入前的占空比。查看原理图,删除D1~D6二极管,删除C23/C33/C28以及R10/R14/R6改为0欧姆,现象依旧
Hi
电机这一块我不熟悉,这个论坛主要讨论电源芯片。
所以之前建议你在主控芯片上问一下。