Other Parts Discussed in Thread: LM5001
各位大神:
上图是LM5001的原理图,设计的输入电压是48V,输出电压是50.67V。但是上电启动的瞬间,输出电压突增到62V。然后回到正常值,还请大神帮忙看看,是不是小弟选的阻容值有问题啊。万分感谢啊!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM5001
各位大神:
上图是LM5001的原理图,设计的输入电压是48V,输出电压是50.67V。但是上电启动的瞬间,输出电压突增到62V。然后回到正常值,还请大神帮忙看看,是不是小弟选的阻容值有问题啊。万分感谢啊!!!
Hi
你的环路补偿有问题,C1不应该是10uF, 而应该是nF级别的。
你可以换成2.2~3.3nF看一下.
Hi
建议你用TI的webench仿真来确认你的电路参数: http://www.ti.com.cn/product/cn/LM5001?keyMatch=LM5001&tisearch=Search-CN
你好 使能EN是要把EN拉低吧,但是我EN脚接地,还是会有电压输出,只是要比正常使能EN低一些
你好,应该不对的,你可以参考datasheet 8.1.3设计电阻让变换器在46V左右才开始工作,然后把电压慢慢加上去,看现象。不过你的补偿参数确实也是太慢了。