This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54302: TPS54302DDCT器件, 输入24V,输出12V的应用。在低温环境-10度下,驱动不起负载,接上负载后12V输出变为4.3V。在高温环境下能正常输出到12V2A。

Part Number: TPS54302

我的应用电路是24V转12V输出。

在高温70度的环境下,能正常输出带动12V/2A的负载,测量电压基本没有压降。

在低温-10度的环境下,接上12V/0.5A的负载,设备会反复重启,测量电压12V跳4.3V然后再跳12V。在低温-10度的环境下,将输入电压24V降到12.5V之后,输出能正常带动12V/2A的负载。

这个是什么问题,请问你们遇到过吗?感谢!