This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: RSOC跳变问题

Part Number: BQ4050


各位工程师好,咨询一个关于BQ4050电量计RSOC跳变的问题;

   4.2Ah 4S2P电池包   使用固定DOV0,EDV1/2动态调节的方式,2.5C末端跳变6%,5C末端跳变22%

                                     使用固定EDV0/1/2方式,5C从33%跳到7% 即EDV2点,且此方式在5C下FCC更新数值只有3700-3900左右,FCC偏小很多

请问一下BQ4050使用在大电流放电的场景下应该怎么调节电量计,防止跳变并保证精度呢?

  • 您好,CEDV 模型的基本思想是电池两端电压 V(SOC, I, T)等于电池开路电压 OCV 减去 电池内阻造成的压降 I×R。大电流放电会导致电量跳变。

    建议用CEDV算法,用小电流充饱以后跑几个循环更新DEV的参数,能减小跳变。