This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: Learned Full Charge Capacity 参数有何意义?

Part Number: BQ4050

 这个参数需要在我做充放电学习时写入吗?它有何意义?

  • 您好, 设置参数的目的是使芯片准确计算容量。

  • 说得太好了,但是我想问的是:这个参数需要在我做充放电学习时写入吗?依据什么写入?

  • 您好,For CEDV the defaulted values are 3V to 4.2V, but these are almost always changed for each application. The TC/FC/TD/FD settings are all dependent on the application so it depends what they want the behavior to be.

    如果您不确定怎么修改可以使用默认参数.

x 出现错误。请重试或与管理员联系。