Other Parts Discussed in Thread: TPS629210
使用TPS629210-Q1设计了一个12V转3.3V电路,电路图如下:

开始时R16和R22均为249K,R14、R20为OPEN,U8输出,U9未输出,上电时直流电源电流大,很快TPS629210的VIN和SW引脚短路。+12VD来自TEN_20-2412WIN

然后将R16和R22更换为OPEN,U8可以正常工作,输出3.3V,但给U9 EN端加3.3V的控制电压时,直流电源又变大,同样TPS629210的VIN和SW引脚短路。
设计参考的datasheet,不能确定为什么会出现这样的情况,不知跟电感的选型有无关系,电感是Wurth的7447732022, 2.2uH。
pcb如下: