TPS54360DDR在使用的过程中,出现的开关频率超差的问题,考虑了RT设定电阻的偏差,以及IC内部控制10%的偏差。但实际测定的开关频率还是超出了这个范围;RT电阻设定是160k+160k+68k(精度±0.5%)的电阻,实际测定大的开关频率是286kHz。(开关波形无抖动);请问这种情况正常吗?在设计的时候,IC本身的偏差考虑为多大算是合理?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS54360DDR在使用的过程中,出现的开关频率超差的问题,考虑了RT设定电阻的偏差,以及IC内部控制10%的偏差。但实际测定的开关频率还是超出了这个范围;RT电阻设定是160k+160k+68k(精度±0.5%)的电阻,实际测定大的开关频率是286kHz。(开关波形无抖动);请问这种情况正常吗?在设计的时候,IC本身的偏差考虑为多大算是合理?
HI
用一个1%精度的电阻来做看看,不要用三个电阻串联,并且选用更高精度的电阻。
您好,感谢回复;
已经了排除了阻值和电路板走线的问题,实装的电阻已经测定了阻值;我更换了其他批次的电源IC,在相同电路和相同电路板的情况下,测定的开关频率是265kHz;又将“出现问题”的IC实装到了另一块电路板(电路相同)上,测定开关频率依旧是286kHz,所以可以判定是电源IC的问题;
顾,有此一问,在设计的时候,IC本身的设定开关频率偏差应该考虑多少%?10%?15%?20%?
Hi
正常都是10%以内。
是所有芯片都这样? 还是少量不良?或者是样板? 请问芯片是哪里买的?
非少量,是量产中出现的问题,同批次出现了二十台以上的机器超差,以前也出现过相同的问题,但是本次不良有些高;芯片的购入渠道是艾瑞
HI
有问题的,如果确实验证芯片频率超出范围是可以联系渠道商的,
只是频率margin即便在20%左右影响并不大,只要是稳定的频率即可,如上你需要确认RT脚的电阻,以及其GND的影响。