This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LDO芯片TPS7A4700/TPS7A3301的输出电容选择和纹波的问题



用TPS7A4700/TPS7A3301做了个+/-15V的双电源,输入是LM1084-ADJ产生的+/-18V电源,纹波有两部分:低频的大概20mV,和尖峰脉冲。经过TPS7A4700/TPS7A3301以后还有10mV左右的低频和尖峰,有以下几个问题:

1.这两个LDO不是说电源纹波抑制比在55dB以上的么?怎么输出纹波差不多是同个量级的呀?

2.输出电容到底应该选择ESR的要求是什么,数据表里说的是越低越好,但从零极点配置上讲,太低的ESR是会引起振荡的啊~ 看了很多资料都说是ESR需要在一个范围以内才稳定,否则就会有振荡的。另外在具体类型上选择哪种电容呢?布局上各自有什么要求?

PS:电路板PCB情况概述,四层板,SIG-GND-VDD-SIG,其中电源层的电源线大概5mm,其余地方也铺地的(+/-15V,感觉电压太高了,加之三四层之间只有0.2mm,所以减少了电源层的面积);主要输出负载:6个DAC,7个AD8675,7个AD8676;输出电容:输出引脚附近各2个0.1u瓷片,3个22u瓷片,1个10u钽电容,每个DAC和运放的电源引脚处附近加一个10u钽电容和0.1u瓷片,电源通路上加一些0.1u瓷片。