Other Parts Discussed in Thread: BQ28400, BQ24170, BQ29200
看了开发板的资料说明,如果想要BQ28400芯片与EV2300连接,需要通过一个转接电路板,我想问下这个板从哪弄?这个板子的设计是开源的吗?
顺便请教下:
BQ24170的OVP电压(输入电压判断)充电之前正常是1.6V,充电时变成4.1V,这个正常吗? 我看指示灯一直亮着,没有闪烁。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The bq28400 comprises three hardware components: the bq28400/bq29200 circuit module, the EV2x00
PC interface board, and the PC.
借助 EV2x00 接口板和软件,用户可以读取 bq28400 数据寄存器、对适用于不同数据包配置的芯片组进行编程、记录循环数据以便进一步评估
所以我想问下,我自己画的电源板要想用EV2300配置的话,不是要用个转接板连接到PC上吗?
我引出的线是SMBUS两个线,GND,还有两根V+,V-