This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5146: 空载情况下,电感发热严重(可达100℃,热成像测试)。

Part Number: LM5146

1、硬件设计:采用官方开发板打样。

LM5145EVM-HD-20A 

2、物料选型:除电感外MOS为原设计同款。

3、调试:

(1)试过多种类型的电感,空载功耗都在100mA左右,并且电感温度都在持续上升。(输入48V,输出24V)

(2)更换电感,DCR从6,9,20都试过了,依旧发热严重,只是温度上升快慢有区别。(电感为10uH,开关频率从100K到500K都尝试过了并无明显区别)。

(3)使用 Webench 生成过参数表测试,依旧电感发热严重。

(4)除了电感发热外,其他元件基本都在40℃。

不知道是哪里出了问题,测试了带载能到200W,并且纹波也无异常。