This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS929120-Q1: TPS929120-Q1:输出45mA时,dropout为0.83V,超出了0.7V的范围

Part Number: TPS929120-Q1

在我们的应用中,输入电压比较小,对dropout比较敏感。

采用数据手册第7页推荐的参数R(REF) = 8.45 kOhm, CONF_REFRANGE = 11b, DC=38,I(OUTx) = 45 mA测量Dropout,测得的Dropout为0.83V,超出0.4V~0.7V的范围,同样,在75mA的条件下测量得到dropout为1.04V,同样也大于1V。想问下具体的原因是?