请问,功率1000W;DC300V转DC14V,驱动部分、mos管型号和评估板一样,死区时间实测200ns,加300V电压,空载,上电就烧mos,四个管全部击穿,后臂上管的泄放二极管击穿,请问这有可能是什么原因。还有我们做单片机控制,是先上高压电还是应该先让28950工作?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问,功率1000W;DC300V转DC14V,驱动部分、mos管型号和评估板一样,死区时间实测200ns,加300V电压,空载,上电就烧mos,四个管全部击穿,后臂上管的泄放二极管击穿,请问这有可能是什么原因。还有我们做单片机控制,是先上高压电还是应该先让28950工作?谢谢
确认一下变压器的设计,可以先给高压,再启动UCC28950.
可以吧电路图设计传上来看一下吗?
请问你的测试是在轻载还是直接1000w负载,建议先用轻载测试。
是轻载,第一回是从空载每次50w往上叠加,加到150W炸的,第二次是空载上电就炸了
我用的是28950,带同步整流,我打算按你说的 先把同步整流部分去掉,谢谢
200ns 会不会太小了?
要在4/1谐振时间里实现开关转换时最好的
建议调试期间加大死区,算下你的谐振周期以及你的谐振电感电容 延后再来 调整合适死区