This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61022: TPS61022开发板配合超级电容使用问题

Part Number: TPS61022

最近项目需求断电后维持对16W负载3s的工作时间,搭建如图所示的电路来进行验证,采用的是TPS61022EVM-034开发板配合超级电容进行调试,想问下各位大神,为什么上电后升压模块无法正常带动负载,输出只有1.8V(外部5V电源功率为150W)。
如果上电前先断开负载,等待超级电容端电压被充满后,再让升压电路对负载输出,此时升压模块能够正常输出5V,但当工作一段时间后电容电压一直会下降,升压模块就只能输出1.8V了
为什么带了负载之后超级电容两端的电压就充不上去了呢,感觉是超级电容一直对负载进行放电。

  • HI

      "上电后升压模块无法正常带动负载", 请问此时输入电压多少?最好是能将启动瞬间的输入波形放上来看看(测试点是芯片Vin)。

      注意这款芯片启动之初需要输入大于1.8V, 芯片正常启动后输入电压可以降低到0.5V.

x 出现错误。请重试或与管理员联系。