你好!在进行文件学习的时候,Cycle Count参数跟新很快,两个循环后Cycle Count=107.请问为什么会跟新这么快?应该怎样避免。而且Update Status一直等于05.跟新不到06或0E。用BQ34Z100-G1最终Update Status能更新到06还是0E呢?在05更新不上去是什么原因?化学ID是TI回传的。有写进去。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!在进行文件学习的时候,Cycle Count参数跟新很快,两个循环后Cycle Count=107.请问为什么会跟新这么快?应该怎样避免。而且Update Status一直等于05.跟新不到06或0E。用BQ34Z100-G1最终Update Status能更新到06还是0E呢?在05更新不上去是什么原因?化学ID是TI回传的。有写进去。
您好
1,CC threshold一般设置design capacity的90%
2, RDIS就是RUP_DIS: If set, the gauge cannot determine its current state and calculations, and will not update the battery resistance tables with its presently measured data. It is cleared when a good OCV measurement is taken, as the gauge acknowledges the absolute state of charge based on this value.
3,静置时间长没有影响