This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: 关于电量计运用指导的疑惑

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQSTUDIO, GPCCHEM

你好!手册里面有几个疑惑的地方,请帮忙解答一下。

在 2.3.5 电量计 Golden Learning 易错分析小节:

• Qmax 不更新的可能原因分析

(1).阻抗跟踪算法未开启,请检查 IT Status [QEN] = 1, Manufacturing Status [GAUGE_EN] = 1。---关于 IT Status [QEN] 这个寄存器,我的理解是对应:【Registers】---【Bit   Registers】-----【Control Status(low)】---【Bit0(QEN)】,请问是不是这样理解。

 ---- Manufacturing Status [GAUGE_EN] = 1,请问这个寄存器在哪个位置?

(2).FLAGS[FC]=1,电池电压taper voltage,是不是实际电压?比如电池电压4.2V,实际要充满到4.2V就可以。在bqStudio工具里面没有看到这个位。

  电流要小于 taper current,是不是指:Data Memory---Configuration----Charge Termination---Taper Current ?

• Ra table 不更新的可能原因分析

(2).[RDIS]=1,这个是不是指【Registers】---【Bit  Registers】-----【Control Status(low)】---Bit2(RUP_DIS),请问是不是这样理解。

正确的 CHEM ID,TI工程师回传了GPC_report.txt文件,我的匹配依据是:从GPC_report文件里面选择了单个电池容量和电池电压 一样的ID。比如我的电池容量是2600mAH,电池电压4.2V.我就选择[Chemistry ID] ---[2188],参数是【Model(1.0(2600mAH))】,[Description(LiMn2O4/carbon,4.2V)]。请问这样匹配对的吗?

  • 您好

    1, Manufacturing Status [GAUGE_EN] = 1就是IT Enable 

    2,请参考TRM 3.7 Charging and Charge Termination Indication 

    3,是的,RUP_DIS: If set, the gauge cannot determine its current state and calculations, and will not update the battery resistance tables with its presently measured data. It is cleared when a good OCV measurement is taken, as the gauge acknowledges the absolute state of charge based on this value.

    GPCCHEM 报告会推荐Best chemical ID