你好!
我配置OCD3的阈值的时候,写入-900写入的值为-900的补码,自定义用户电流单位为10mA,但是电流给10A的时候,并不会发生故障,此时OCD1 OCD2 OCDL都已经故障了,请问一下是什么原因
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,There are some of the FET commands that cannot be used for controlling the DDSG and DCHG pins. See the descriptions in Table 5-8 of the TRM below.

The ALL_FETS_ON() and ALL_FETS_OFF() commands should both work, and the CFETOFF and DFETOFF pins can also be used to control these outputs.