This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: Balance 问题咨询

Part Number: BQ76930


Hi 

单板已经校准过,单节最大值减去最小值在10mv已内,在组装电芯后读取电压后,会显示单节最大值减去最小值远大于10mv的情况(例如31mV.

实际测量 1~5节电压偏小,6~10节电压偏大。

请帮忙看下什么情况会导致这种情况。

另外,请问下各电芯之间电压差最高是多少 ,认为是没问题的? 我看规格书内BQ76930 Icb 最大是5mA , Cell balance driver 是5ohm典型值,最大10ohm, 是否可认为压差值最大是50mV,超过这个值会进行保护 ?