This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS552892-Q1: 空载电流过大的问题

Part Number: TPS552892-Q1


以上是我参照TI的DEMO板出的图,输入9-24V,输出12V,在未带负载的情况下,输入12V,空载电流大概只有10mA左右,当我把输入调整到11V或者13V(这两种情况输出电压均正常为12V),但是此时输入电流会急剧增大,能到100-200mA甚至更高,请问这是什么原因(对L2这个电感额定电流有要求吗,我选的这个额定电流大概900mA),以上情况都是在输出空载的时候进行测试的,望能回答,感谢!