This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS709: TPS709

Part Number: TPS709


我使用TPS79033,输入12V输出3.3V,电流在4mA左右,SOT32封装的芯片用温度枪看是36度,查看手册看到WSON封装的温度系数比较低

于是采购了WSON封装的进行测试,结果还是在36度。基本没有变化,请问这个正常吗?

有没有其他方案能在入12V输出3.3V,电流在4mA左右,温升低一点,因为要和温度传感器灌封在一起所以温度比较敏感,但是体积也不能太大,因为壳体的限制