This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

用LM5116设计12V电源板,过载后去掉负载,输出12V不能恢复,并且LM5116的晶振以及HO,LO频率降低一半的问题!!

Other Parts Discussed in Thread: LM5116

1. LM5116为核心实现电源管理的12V电源板,输入40~80V,输出12V,保护电流3.7A,SYNC晶振频率300KHZ,开始使用15UH电感,带正常输出12V,带负载,电流大于3.7A,过载保护输出降低到9V,去掉负载后能恢复12V正常输出,性能基本可以,只是输出12V毛刺大,约8Vp-p

2. 为了降低输出12V电压上的毛刺杂波,将电感更换为33UH后,带正常输出12V,带电流大于3.7A过载保护输出8V可是不到几秒钟很快输出降为0V,随后去掉负载,空载后再也不能正常输出12V ,输出仅仅3~4V,此时测量SYNC脚,HO,LO脚,已经没有300KHZ方波了,只有一些杂波很乱,测不出频率

3. 更换新的LM5116,空载可以输出12V,此时LM5116SYNC管脚以及HOLO管脚的频率均由原来设计的300KHZ降低一半成为150KHZ。检查电路板上LM5116SYNC脚的外接电阻值并没有变化,附录图中SYNC外接电阻R710k,R13150Ω串联的电阻阻值没有任何变化,此时空载输出12V,但是不能带负载,对外围电路逐一检查,更换各个电阻电容,但没有什么变化,频率始终是150KHZ,空载时输出仍然是12V,但是不能带负载,带负载电压降低到3V左右,并且带负载后LM5116的SYNC,HO以及LO管脚的150KHZ方波会变成没有一定频率的杂乱波。

    请问是哪个外围元件参数发生变化才导致LM5116SYNC频率降低一半(LM5116是更换新的芯片)?原因是什么?请各位TI技术支持指教,谢谢!!

以LM5116为核心的12V电源板原理图.pdf