This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: bq76952体二极管保护body diode protection

Part Number: BQ76952


bq76952的体二极管保护,能查到设置阈值的地方,但从检测到电流,到执行FET的控制,消耗多长时间,没有标注

请问,是否可以设置延时,如果不能设置,响应时间是多少?

  • 您好,There is not a way to modify the timing you describe. The body diode protection is decided by the firmware. There is a table showing the timing for many events in Table 6-9 of the TRM. The timing for this event is most likely on the 250 ms timer on which the conditions for the FET states are evaluated.