Other Parts Discussed in Thread: TPS54340

原理图如图,芯片底部裸露铁皮为25脚EP,连接到地。
5v输入,电感啸叫,并将5v输入拉低到2.5v,三极管Q1集电极和发射级电压一样,都是2.5V,本应输出15v的地方输出7v,本应输出-10v的地方输出0.7v。
将电感L2、电容C45去掉,并将15引脚连接到地,啸叫问题消失,能正常输出3.3v电压,但仍无法输出15v与-10v电压,这两个位置输出的都是0.7v,请问哪里出问题了呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
确认一下功率电感饱和电流是否足够? 注意输入电容尽量靠近电感输入端?
其次确认一下输入源5V是否有电流限制问题?
您好,确认是芯片损坏了,更换芯片后,我设置R29的值为470K,意在使升压输出为10.5V,并更换COMP引脚的补偿电阻R30为3.3K,可以正常输出所有电压。但设置R29为620K,意在使升压输出为14V时,虽可以输出14V,但电感啸叫,输入的5V又被拉低到2.5V,此时加大补偿电阻R30和补偿电容C8,问题依然存在,而R29的值我也不敢再加到680K,怕一通电芯片又烧了,请问这种情况是我COMP引脚的补偿不合适吗?要使升压输出15V,设置补偿电阻R30和补偿电容C8的值为多少合适呢?