Other Parts Discussed in Thread: BQ25618
Hi ti team,
我客户在使用BQ25618EVM测试时,遇到两个问题:
1,IC进入CV模式,充电电流在50mA时会有一个微小的突变,请问这是什么原因造成?

2,当电池电压在3.5V左右时,插入Vbus,充电电流会有短暂上下跳动(1S以内),请问这是什么原因造成?如下图

寄存器配置:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ti team,
我客户在使用BQ25618EVM测试时,遇到两个问题:
1,IC进入CV模式,充电电流在50mA时会有一个微小的突变,请问这是什么原因造成?

2,当电池电压在3.5V左右时,插入Vbus,充电电流会有短暂上下跳动(1S以内),请问这是什么原因造成?如下图

寄存器配置:

您好,请参考下面内容
1. Please provide more background information for these observations. What was the input voltage and battery voltage, was there a system load, how repeatable is this, was this seen on other device etc? Was the device in DPM? Please check the status when this happens.
2.The root of the observation is the BATFET turns off between linear mode and switching mode. The charger gets out of this scenario because the average current is positive. Please lower your PCB trace impedance and battery impedance to fix this issue. If possible lower VSYS_MIN to reduce the transition time to switch from linear mode to switch mode.
Hi Star,
1. Please provide more background information for these observations. What was the input voltage and battery voltage, was there a system load, how repeatable is this, was this seen on other device etc? Was the device in DPM? Please check the status when this happens.
VBus输入电压5V;电池已经进入CV状态,电池截止电压为4.45V;使用TI EVM板在测试,后端没有拉负载;BQ25618未进入DPM状态;这种现象每次都会出现
您好,已经在E2E英文论坛发帖,暂时没有收到回复,请继续关注该帖。