您好,我想请教一下PSE芯片(TPS23861)的数字地与模拟地没有接在一起(且数字地与模拟地是隔离的,没有接在一起)这样设计可以吗?,下图是我参照数据手册绘画的原理图,图中48V输入是板卡的输入源,该输入通过一个电源模块将板卡内部的地(数字地)隔离开来,绿色部分是我按照数据手册上给的提示,接入的板卡输入的模拟地,蓝色部分是接入板卡内的数字地,请问这样设计PSE芯片能正常工作吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
请教一下PSE芯片(TPS23861)对外部非PD设备供电的问题,我们有需求需为非802.3axxx 负载(即没有 PD 的负载)接通电源,负载需要40W左右的功率,我们采用手动模式,关闭端口检测分级功能(利用I2C操作寄存器0X14),更改ICUT (mA)电流为754mA(或者是最大阈值电流920mA), 我们VPWR供电54V,所以
最大功率输出①: 54*0.754=40.7W 或者
最大功率输出②: 54*0.920=49.68W
通过操作寄存器0X19来对端口供电进行打开与关断,请问您我们这样设置,能达到我们所需的高功率(40W)供电需求目吗?
如下图所示,红色框内并不是一个RJ45,是一个两个孔的电源接口
Hi
具体的操作控制建议你在美国E2E上问一下。那边有这个芯片产品线的工程师,他们应该有调试经验。
(我主要是熟悉电源设计,我们这边没有这个板子调试TPS23861, 没有具体的调试步骤)