This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76005: LM76005输出电流无法达到12V5A

Part Number: LM76005


使用LM76005,Vin=48V,Vout=12V,使用电子负载进行测试,发现当Iload>1.5A时,芯片会间隔60ms重启。

当通过调整电阻使Vout=1V时,Iload=5A,芯片输出正常.

请帮忙分析一下我的电路存在什么问题导致无法输出12V5A?