Other Parts Discussed in Thread: BQ76930
BQ78350-R1A的设计中,DF的setting中,Manufacturing中的Mfg Status init的设置会自动清除掉,变成0000,请问大概是什么原因。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ78350-R1A的设计中,DF的setting中,Manufacturing中的Mfg Status init的设置会自动清除掉,变成0000,请问大概是什么原因。

但是我使用右边的命令框,又可以一项项使能,不知道什么原因,我现在用的是R3的固件。之前可以直接在mfg中设置。

在调试的过程中,发现一直有电流存在,导致系统判断为充电或放电,这个电流是怎么产生的,是否为元件损坏造成的。

可以校正,但是,我按一下DISP,没有加充电器,电流自动变成了40mA,然后显示在充电。我把静态电流阈值改50mA,就没有显示充电了,但是电流还在。同时,均衡自动启动了,但实际上我是把均衡关闭了。我猜测这个40mA的电流是均衡电流。但是我这边电池只有3.6V,没有达到均衡的条件。
我检查了所有的电路,没有发现问题,但是,发现启动了均衡,我按下DISP按钮后,均衡启动,但是我明明关闭了均衡,这个和BQ76930是否关联。
下图是电池电压,发现1S一次,电压下降和升高,时间为100mS.不知是触发了什么电路。

感觉进入了均衡状态,然后当前LED灯一直闪。充电标志位并没有显示在充电,很奇怪呀。按理说应该应该到3.9V以上才均衡。难道休闲也进入了均衡?还是说DISP有启动均衡的作用?

您好, It is not unknown that LEDs draw current. I see that there's a 100Ohm resistor in the LED path, see below for the EVM schematic. The 100 Ohm might be current limiters, but could be dissipating power.

What can be done is increase the Deadband to 50mA. This will inform the gauge to report 0mA for current less than 50mA. It has no gauging effect since the coulomb count will reset as I see the current going positive and negative, so the accumulated charge cancels out.
| Calibration | Current Deadband | Deadband | 3 | mA | U | 1 | 792 | 3 | 0 | 255 | ddd | x+0 | x | mA | 0x03 |