通过单片机配置data flash时,在0x00写错了命令,现在sbs可以读,但是data flash读不了,什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电量计为sealed 状态,
需要解锁,
To enter Full Access mode from Sealed mode in CMD (0x61), enter the 1st and 2nd bytes of the words as 0xffff and 0xffff. This instructs the bq28400 to allow Full Access to all SBS commands and data flash. The bq28400 is shipped from TI in this mode. The key for Full Access can be read and changed via the extended SBS block command FullAccessKey when in Full Access mode. Use the ManufacturerAccess command to change from Sealed to Full Access by writing the 1st word of the FullAccessKey to ManufacturerAccess followed by the second word of the FullAccessKey to ManufacturerAccess. The full access key can be read and changed via the extended SBS block command FullAccessKey when in Full Access mode. In Full Access mode, the command to go to Boot ROM can be sent.
请用FullAccessKey 来解锁