This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,Just to confirm whether this is an issue with the ADC calculation, can you provide the raw ADC measurements from while the device is exhibiting this behavior?
You can find the registers to get these values from Section 4.6: Subcommands 0x0075–0x0077 DASTATUS5–7(), Additional Measurements of the TRM.
只会平衡使用中的非相邻电池。
您好,The device allows for host-controlled cell balancing. The device does not have a programmable timer for the balancing duration. This is explained in Section 4 of the Cell Balancing application note.
您好,温度的问题已经在E2E英文论坛发帖,请继续关注下面的帖子
您好,建议您使用thermistor coefficient calculator 工具重新计算温度相关的参数来满足您的温度需求。
详细的步骤请参考下面FAQ的帖子