专家好:
TMS320C6678 EVM Board 开发板上面UCD9222的PMBUS接口采用的是6针的插针,可是Fusion Design 采用的USB ADAPTOR的采用的是10PIN插头,是不是这两个之间还需要个转接板?如果不需要的话,有没有6PIN的下载器呢?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
专家好:
TMS320C6678 EVM Board 开发板上面UCD9222的PMBUS接口采用的是6针的插针,可是Fusion Design 采用的USB ADAPTOR的采用的是10PIN插头,是不是这两个之间还需要个转接板?如果不需要的话,有没有6PIN的下载器呢?谢谢
Xin Lee,
UCD9222支持JTAG和PMBUS下载,具体参考附件。下载线可以在TI的电子商店购买:estore.ti.com/USB-TO-GPIO-USB-Interface-Adapter-EVM-P960.aspx
前辈你好,
在TI 论坛上看到了你的帖子,有以下两个问题想问下你:
1)如何在烧写前检验Digital power Designer的配置文件是否正确?
2)我的Digital power Designer 中没有导出x0格式文件的选项,这是为什么?那如何对UCD9222进行烧写呢?
您好,您是否已经成功解决UCD9222程序下载问题,想请教您,谢谢。