This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
没有哪个脚损坏,是芯片有最大占空比限制功能,根据外围参数计算,最大占空比能到72%, 但是实际只能到66.4%(好的芯片能到70%) 导致输出电压偏低。不良率比较高,而且有些批次性比较严重,我们又无法筛选,如:DC:2244(SMT),不良数量:19pcs,不良率:19/858=2.21%, 所以发给TI 分析。谢谢!
Hi
将正常板子和异常板子芯片对调,确认异常是否跟着芯片走? 如果是就是芯片的问题,如果不是很可能是反馈的问题。
跟着芯片走。换了其他芯片就好,换回来又差了。不好的芯片换到其他板子上也是不好的。