Hi
请帮忙推荐颗横流芯片。规格如下,竞争对手型号:SF6771S.
我们需要找一颗恒流控制型的DC-DC芯片,VIN≥35V,输出功率大概30-50W,频率:300K以上,输出可调,带EN使能,控制MOS外置,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
请帮忙推荐颗横流芯片。规格如下,竞争对手型号:SF6771S.
我们需要找一颗恒流控制型的DC-DC芯片,VIN≥35V,输出功率大概30-50W,频率:300K以上,输出可调,带EN使能,控制MOS外置,
Hi Johnsin:
输出电压也是大概24V 左右,是给8S 的磷酸铁锂电池充电用。 应用场景是8S磷酸铁锂电池,通过DCDC 升压起来给另一个8S磷酸铁锂电池充电。
Hi
如果充电的话,直接在电池管理论坛上提问选型。
Hi Johnsin:
客户不是要充电管理IC, 是想找个恒流DCDC 自己来做充电功能。帮忙确认下是否有满足规格的横流DCDC.
HI
如果是要设计恒流设计,很多DC/DC都是可以的,例如LM3150之类都是可以的,只要将常规的通过电阻分压反馈改为通过运放侦测sense电阻做恒流设计即可。
但这类DC/DC,和类似SF6771S的反激芯片差别很大。