This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61089: TPS61089的RILIM应当怎么计算,手册中给的8A电流时的127K,但是WEBENCH设计的3.5A的电阻是110k

Part Number: TPS61089


我现在是需要3.5A的电流(实际整个电路工作在1.5A),应当使用这个110K的配置吗