This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25504: 当输入电源内阻较低时,MPPT工作不正常

Part Number: BQ25504

您好:

我想要使用BQ25504进行热电能量收集,我的热电片输出情况预计为250mV,等效内阻为2Ω,我使用一个250mV的电压源通过一个2欧姆的电阻来等效热电片与BQ25504的VIN_DC引脚连接,BQ25504电路的原理图如下

输入电容Cin选择手册推荐值4.7uF瓷片电容,Vstor接的是一个4.7uF电容,Vbat接的是一个1.5F超级电容,已经被预充电至2.9V

MPPT比例设置为50%,我希望看到的情况是VIN_DC引脚平均电压为125mV,电压源的平均输出电流为125mV/2Ω=62.5mA,但是实际的情况是VIN_DC平均电压为175mV,平均电流为38mA,VIN_DC(CH1)和LBST(CH2)引脚的波形如图所示

起初我猜测是输入电容较小导致输入电压纹波较大,导致输入电压不能得到很好的调节。于是我将输入电容换成47uF,情况得到了一些改善,VIN_DC(CH1)和LBST(CH2)引脚的波形如图所示输入电压平均值变为159mV,平均电流变为46mA,但是继续增大输入电容虽然能减小纹波,但是输入电压电流的平均值不会改变。

降低MPPT电阻的分压比例也不会使波形有任何改变

将输入电阻改为3Ω后,输入电压平均值为140mV,最小值为125mV,因为手册描述输入电压调节率为±10%,所以我认为此时MPPT工作比较正常

综上,我想请教一下,当输入电压250mV,等效内阻为2Ω时,BQ25504的MPPT工作不正常是因为什么原因,在输入条件不变的情况下是否能够使BQ25504得到最大功率输入(VIN_DC=0.5*250mV=125mV)。

谢谢