This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: 在16串电池电压高过52V后,PACK+的输出电压限制在52V左右问题。

Part Number: BQ76952


Hi,

在16串电池电压高过52V后,无论多大,PACK+的输出都是限制在52V左右,此时CP1的升压也从11V降低到不足1V。

即使外部切断了DSG和CHG,以及PDSG和PCHG和MOS的连接也一样。增大电容到2.2uF也没变化。

软件上在正常模式和测试模式下在初始化后,使能FET前CP1电压还有近11V,使能FET后就降为不足1V了(电池电压52V以上时)。

希望能尽快得到帮助,多谢了!