Other Parts Discussed in Thread: BQ25170
当温度达到某个值时,TS的电压超出阈值范围,LM3658关闭了充电进程,此时由于重载变空载,导致TS的电压抬升了40mv左右,又落入了阈值范围内,LM3658开启充电进程,TS电压又被拉低,进而关闭充电……如此反复,造成在某段温度范围内,充电IC反复开启充电和关闭充电,请问是否有能改善TS电压波动的方法。
图中通道1黄色信号代表TS引脚电压,通道2蓝色信号代表充电状态,高电平开启充电,低电平关闭充电。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,This is a legacy device and so unfortunately we don't have too much information available about this part, we typically recommending looking at newer components. The BQ25170 family offers similar simple implementations, though the power mux feature may be needed from a separate IC.
Is the battery heating up significantly during charging? The current used to bias the NTC should be constant regardless of charging.
您好,As mentioned before, unfortunately we don't have too much information available about this part. I would check if the spikes in voltage correspond to any changes in input or output voltage as well as changes in current other than charge current to try to identify the cause.
It appears that it only occurs while the charger approaches the low-temperature voltage threshold, I'm unsure the level of hysteresis that was put in place for this device.