This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24073: 充电截止温度

Part Number: BQ24073
Other Parts Discussed in Thread: BQ24072, BQ24075, BQ24075T, BQ24072T, BQ24079T, BQ24079

您好!

我在使用BQ24073时,其中PIN1接到电池的NTC,电池的NTC阻值为10K,现在实际测试在高温环境下,电池的充电截止温度为57°C,我们现在期望的充电截止 温度是45°C,想请问下可以从哪些方面做调整?目前我们的电路设计如下图:

烦请帮忙解答,谢谢!