1.如图中大于1.2Mhz频率下,有最小负载电流限制问题,TPS55340最大开关频率应当是1.2M吧。
2.关于最小负载电流问题,目前需要通过1hz的三角波电压驱动图中所示的电路,计划使用TPS55340作为升压模块供电,通过仿真,路径电流在uA级别,TPS55340还能作为升压模块吗?
若能指点,非常感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
你可以将频率设置到1.2MHz, 但是电流非常小,如uA, 芯片会进入较高效率的脉冲跳跃模式,这个时候频率会降低。只有重载下芯片进入固定频率PWM模式。