This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用PTH08T240W的Turbo Trans功能时瞬态响应很大

Other Parts Discussed in Thread: PTH08T240W

我在使用PTH08T240W的Turbo Trans功能时,输出VO接了3个100uF陶瓷电容(ESR=2毫欧),2个47uF陶瓷电容,
满足电容 type A : 100≤C(μF) x ESR(mΩ) ≤1000 。
输出负载从1A到5A周期变化,频率为1000HZ,占空比为50%,输出电压波形如下图所示(200mv/div,200us/div),电压偏差很大>400mv
外接电阻RTT(从9脚TurboTrans到6脚+Sense)从0K增大到200k测试时,输出电压偏差还是很大>400mv

是测试方法不对吗?(示波器探头直接测试的模块电路输出脚)
请问怎样减小瞬态响应的电压偏差?